Other Parts Discussed in Thread: DAC7625, DAC7725
Hi,
I was just wondering what is the maximum output voltage of the DAC7625, a former burr-brown device.
The datasheet says the output voltage can't be higher than REFH, whereas REFH has a maximum of 2.5V. Thus I would say 2.5V is the maximum.
BUT, according to the TI product page the output voltage range is -10..+10V.
Is it possible to drive the DAC with an output voltage of +10V???
Appreciate your help!!!
Thanks
Michael