Other Parts Discussed in Thread: ADS52J90EVM, ADS52J90
Been asking questions over on Medical forum but not getting any useful answers.
Have ADS52J90EVM & TSW14J56EVM running.
Using external clock through ADS52J90EVM J75. Just guessed at 1 V p-p sine wave for input clock; can't find anything about this in documentation. Would like to use onboard 100 MHz oscillator, but can't find instructions for doing this. Some info about jumpers in doc, but no instructions. Probably also would need to reconfigure LMK chip. How?
Want to run converter as JESD output, 4 lanes, 10x, 10b. There are a bunch of .cfg files, but not one that corresponds to this. Can this be done on this eval board? ADS52J90 should be able to run in this mode.