DEARS.
We are considering the AFE7225 for the new project.
There are several questions about the AFE7225.
Answer please.
Q1. Is Lo Freq possible that each DAC and ADC set up?
Q2. ADC is 125MSPS, possible range of Band is from 0Mhz to 62.5Mhz?
Q3. DC Offset measurement data is needed. DC Offset can you get the data?
Q4. What is the maximum power consumption of AFE7225?
Q5. What are the features and the detailed description of the structure of the FIR?
Q6. what is ADC dynamic range of input and output?
Q7. what is DAC dynamic range of input and output?
Q8. NF measurement data is needed. NF can you get the data?
thanks