Other Parts Discussed in Thread: ADS42B49, ADS4249
The ADS42B49 datasheet recommends "Set the HIGH PERF MODE[1:11] bits to obtain best performance across input signal frequencies", e.g. in Table 4, p. 27.
- But -
All the charts are shown with "High-Performance Mode disabled." My question is:
What effect does setting the HIGH PERF MODE[1:11] bits have? in what way is the performance "best"?
(By the way, this is in contrast to the datasheet for the ADS4249, where behavior is charted with "High-Performance Mode enabled." It's also in contrast to my expectations about specs-manship, where I imagine a manufacturer would always put their best performance in the charts.)
My application involves digitizing a relatively low frequency signal (< 10 MHz) with lots of harmonics, e.g. up to 60 MHz, of which I would like to record a reasonably faithful representation.
Thanks for any insights you can share on this.