Other Parts Discussed in Thread: ADS1234, TS5A3166, ADS1232REF, TS3A4751, ADS1231
What is the recomended switch for ads1234 that can be used to break the excitation to the bridges to save power when not converting?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
One possibility is the TS5A3166 when using 5V bridge excitation or less. This device was used as part of the reference design for the ADS1232REF (2 channel version). A MOSFET could be used as well. Generally what you are looking for is low on resistance.
Best regards,
Bob B
Hi,
The MOSFET is less complicated, but switch resistance is a little higher. You can avoid issues with the switch by making sure the measurement maintains the ability to be ratiometric. This removes the affects of the switch resistance from the measurement by making sure that the excitation of the bridge is the same as the reference voltage. You could use something like:
Best regards,
Bob B