Other Parts Discussed in Thread: ADS1248
Hello,
I am using the ADS1248 in the DOUT/DRDY combined mode (DRDY bit set) to limit number of the interface pins. I also perform a single conversion after a SYNC command,so I do not need the continuous reading mode where reading needs to align to DRDY. I noticed that DOUT/DRDY indicates end of conversion only when ADC reads data continuously (default state or after RDATAC command). DOUT/DRDY does not function after SDATAC (stop reading data continuously) command.
Q: Is that behaviour correct, i.e. DOUT combined with DRDY works only in the continuous reading mode?
Best regards,
Robert