This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW1200EVM Board: FPGA Configuration File and UART-USB-Bridge

Other Parts Discussed in Thread: TUSB3410, ADS6445, ADS62P49, ADS5400, FMC-ADC-ADAPTER, ADS5474, ADS5485, ADS5560, ADS62P24

Hello!

I have the TSW1200EVM module and use it to develope a measurement system with the high speed ADC 62P49. The FPGA boot prom contains two fpga configurations to drive different ADC evaluation boards.

Is it possible to get the Xilinx ISE project and *.bit files of these two configurations?


Furthermore I'd like to use the UART - USB bridge that is realized with the TUSB3410 Chip. The configuration to drive the board with the Ti software is stored in the I2C EEPROM named U8.

Can somebody tell me how this program in the I2C EEPROM configures the TUSB3410 (how many bits, baudrate, stoppbits, parity)?


Regards Simon