Are ADC3444EVM and TSW1405 compatible?
Is there anyway to directly communicate with TSW1405 trough C++ and transfer the sampled data of all 4 channels from ADC3444EVM?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Are ADC3444EVM and TSW1405 compatible?
Is there anyway to directly communicate with TSW1405 trough C++ and transfer the sampled data of all 4 channels from ADC3444EVM?
Vahid,
Currently the TSW1405 does not cover the ADC3xxx family. We have some plans to enable the TSW1405 to support the family but at this time that is not yet available. The TSW1400 will work with the ADC3xxx family until the TSW1405 support is available.
We do not have a direct hardware DLL for the TSW1400 or TSW1405. We currently only support an automation DLL which can be used to control HSDC Pro to capture the data and then grab the memory buffers for analysis. You can find information for this in the HSDC Pro installation directory under the automation directory:
C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro\HSDCPro Automation DLL
Ken.