I am using the LMP90080 with 5 thermocouples connected. I all works well except now I need to test for open circuits. I can do this in the normal Mode 3 with Burnout enabled because a use one input as a thermocouple common. So any current injected into the previous TC would affect the one that is being converted. So I need to switch scan modes every so often to single channel scan with Burnout enable and check the flag.
My question is when is the minimum registers I would need to change in order to switch scan modes back and forth?
Thanks,