Running Windows 7 PROx64.
Install as per instructions. TI USB SPI interface not available. No driver, it says.
Go to this forum, read the post shown below. Get the file. Follow the directions. Do not really work as shown. Screens and selections are different. What is shown in the Power Point is not what I see on the screen. Try to follow them as best I could. Seems to install. Changes name of interface to TSW3003. Doesn't work.
OK, officially dead in the water. Development has stopped. Is there help available on this?
Ralph
This previous post
Hello Susana,
Could you try the attached driver installation procedure for WIN7? We have tested this on the TSW3003 EVM (with DAC5687+TRF3703) on WIN7 and USB driver installed correctly.
Regarding the SPI programming directly from the FPGA to the DAC5687EVM, the EVM does not have an external direct connection to the SPI port of the DAC5687. If you really need to do so, you may need to remove U4 and solder down blue jumper wires from your FPGA EVM to pin 18, 16, 14, and 8/17 of U4 location.
-Kang
TSW3003 Driver and Installation Instruction.zip
did not work.