Hello,
I am working with the ADS5401 high-speed data converter. The nominal sampling clock provided to the ADS5401 is a 800 MHz clock generated by the TI LMK04906. The performances of the ADS with a 800 MSPS sampling rate correspond to what we need for our purpose. We have a need to use different clock frequencies, for instance 40 MHz (provided by the same clock synthesizer).
I know that 40 MSPS is the lower limit for the digitization rate (800 MSPS being the upper limit). The performances of the ADS with a 40 MSPS sampling rate is not as good. In particular, looking at the ADS intrinsic noise I observe than the noise shows two distributions, meaning that the noise is going back and forth between two offset values. This behaviour is not seen at all for frequencies above 100 MHz, up to 800 MHz. I am attaching slides (hope it's going to work) to this post to show you the noise problem I am facing, the 800 MHz clock signal, 40 MHz clock signal.
Does the ADS5401 needs a sine wave clock only or is a square wave fine too? The shape of the signal output by the clock synthesizer is changing from a nice sine wave at 800 MHz to a square looking wave at 40 MHz. Could it be an issue? The amplitude of the clock are also different but I do not see why it would be an issue according the ADS data sheet.
Thanks in advance for you help!
Antoine.