This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC128S085 DOUT level

I don't see the DOUT voltage level (VOH) called out in the datasheet. There's an output voltage section, but I believe this is just for analog voltages. If VREF = 2.5V and VA = 5V, can we expect the DOUT pin high level to be 5V? We are using an SPI master running at 3.3V but it does not have 5V tolerant inputs, so we're wondering if we need to add level shifting.

Thanks