This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS129xECG - FE software operating system

ADS129xECG - FE software can only run on Windows 7 32-bit system, will not run on Windows 7 64 - bit systems, is that right?A 64 - bit system USBStyx driver installation is not successful. Is there anyone to support 64 - bit system software?

  • Hi user4592808,

    I'm not aware of any problems running the ADS129xECG-FE software under Windows 7, we'll look into this for you. What sort of error messages are you getting?
  • Under a 64 - bit Windows 7 system, run the ADS129xECG - FE software, libusb0. DLL file is missing, when will download libusb0. DLL files, in the system32 folder, can normal installation software.But only MMB0 driver installed correctly and USBstyx driver didn't get the hint, ultimately unable to connect to the hardware, DSP is not ready.And under the 32-bit Windows 7, do not have this problem。