Brian,
Off late I noticed a lot of noise on the output of the ADS1292 and tried everything possible to overcome that. I changed the setting in the RLD_SENS register to 0x2D to give theRLD drive from all the three electrodes hoping that the increase in the RLDOUT would compensate for the noise. Everything in terms of ambient was same as compared to the time I was getting clean output. Then I checked the resistance of the lead which had marginal increase of 1 Ohm but I did change the lead and got the clean output again. Would the 1 Ohm increase in resistance of the lead make so much of a difference, given the fact that there is a 100K Rp in series with it.
While searching for the solution I also came across a post of yours which said that one should have the a cap of 25.5 nF put in parallel to the Rp to get a 60 Hz cutoff. Can"t i change the cap between the RLDOUT and RLDINV to get the 60 /50 Hz cutoff rather than having it configured as a LPF of 106 Hz? Could you please explain that too.
Regards
Viney Chaddha