This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC34H84EVM GUI BYPASS



Hi every body

I have some problem about byspassed the DAC34H84EVM GUI to program the DAC through the Config regsiter. So for do that i'm using a FPGA stratix 3 with Quartus 9.1 where i built a nios II and a C program to write via SPI mode inside the DAC.

When i remove the jumper JP8, JP9, JP12, and JP13 on the EVM an connect them to the FPGA board i have several mistake in the registers values.

For example:

the Default config of register 0 to 5 is

x00 x049C
x01 x040E
x02 x7000
x03 xF000
x04 x4923
x05 x8560

After load this instruction

alt_u8 temp;
alt_u8 wdata[] ={0x05,0x00,0x00};

alt_avalon_spi_command(DAC34_SPI_BASE,0,3,wdata,0,&temp,0); // is the SPI method to write 3 byte where the first is the instructun byte and the else are the 16 data bits

I have those values

x00 x8383
x01 x040E
x02 x7000
x03 xF000
x04 x4923
x05 x8578

I don't understant nothing for this, the only values that i was expect to change is the values associated with the register 5

Please is there someone who can help me??

Best regards

  • Kemoah,

    I recommend that when you use jumper wire for SPI bus between FPGA board and DAC EVM, please also make sure ground connection between the two EVMs are solid. Otherwise you will have bit errors like you have seen so far. 

    also, register 5 is an alarm register. The error are sticky and may change depend on the operating condition. You will need to analyze the error accordingly.

    -Kang