Other Parts Discussed in Thread: ADS1278, ADS1278EVM-PDK
We are using an ADS1278 and are having some issues with the converted data.
The 1st 3 channels are shorted together. The 1st channel data looks correct. The 2nd and 3rd channel data looks like the sign could be flipped.
We are reading the 8 channels via the pseudo SPI from a SM470R. We read 24 bytes all between the /DRDY pulses.
I will try to get some scope captures.
The problem seems to be very similar to this problem, but it is not clear to me what we can change / tweak:
https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/43479
Please advise.
· End-application - High temp electronics
· Detailed problem description - See above
· What is your input signal - 4.3 Volts
· Supply voltages - AVdd=5V, IOVDD=3.3V, DVDD=1.8V
· Reference voltage- Vref=2.5V
· Input and reference drive circuits - Reference is driven from a REF5025SHKJ, Inputs come from an OPA211SHKJ low pass filter.
· Digital control pin settings (i.e. Reset, PowerDown, Start, etc.) - Format0=1. Format1=0, Format2=0, Clkdiv=1, Mode0=1, Mode1=1, /Sync=1, /PwrDwn=1