This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multi channel bipolar adc required with selectable range

Genius 3300 points

Other Parts Discussed in Thread: ADS8634, PGA281, PGA280, ADS8668, ADS8694, ADS8698, ADS8688A, ADS8684A, ADS8684, ADS8688, ADS8681, ADS8678, ADS8674, ADS8664

1. I have application which require multichannel bipolar adc with selectable range. Below are specs
A) Selectable input range: +-10V,+-5V,0 to 10V, or 0 to 5V.
B) Bits: 12 or higher
C) Interface: SPI preferable not parallel
D) Channel: 8 channel. In case of 4 channel, two adc will be used.
E) Supply: Single supply operation is preferable.

2. I was looking at ADS8634.
Looks like is it ok. Except dual supply is required.

3. Any other recommended ADC.