Other Parts Discussed in Thread: DAC8411
Hello,
I'm currently trying to implement the DAC8411 to output a basic sine wave and I'm running in to a bunch of issues. I am using an Arduino for this project however I cannot see any output and I do not see anything going to high when I use the logic analyzer. Any suggestions? My code can be seen below.
// inslude the SPI library:
#include <SPI.h>
byte sinewave[256] ={
127,130,133,136,139,143,146,149,152,155,158,161,164,167,170,173,176,178,181,184,187,190,192,195,198,200,203,205,208,210,212,215,217,219,221,223,225,227,229,231,233,234,236,238,239,240,
242,243,244,245,247,248,249,249,250,251,252,252,253,253,253,254,254,254,254,254,254,254,253,253,253,252,252,251,250,249,249,248,247,245,244,243,242,240,239,238,236,234,233,231,229,227,225,223,
221,219,217,215,212,210,208,205,203,200,198,195,192,190,187,184,181,178,176,173,170,167,164,161,158,155,152,149,146,143,139,136,133,130,127,124,121,118,115,111,108,105,102,99,96,93,90,87,84,81,78,
76,73,70,67,64,62,59,56,54,51,49,46,44,42,39,37,35,33,31,29,27,25,23,21,20,18,16,15,14,12,11,10,9,7,6,5,5,4,3,2,2,1,1,1,0,0,0,0,0,0,0,1,1,1,2,2,3,4,5,5,6,7,9,10,11,12,14,15,16,18,20,21,23,25,27,29,31,
33,35,37,39,42,44,46,49,51,54,56,59,62,64,67,70,73,76,78,81,84,87,90,93,96,99,102,105,108,111,115,118,121,124
};
uint8_t divider = 24;
// set pin 10 as the slave select for the digital pot:
#define DATAOUT 51 // MOSI
#define DATAIN 50 // MISO //not used
#define SPICLOCK 52 // Clock
#define SELPIN 53 // chip-select
void setup() {
// set the slaveSelectPin as an output:
pinMode(SELPIN, OUTPUT);
pinMode(SPICLOCK, OUTPUT);
pinMode(DATAOUT, OUTPUT);
// initialize SPI:
digitalWrite(SELPIN, HIGH);
SPI.begin();
SPI.setClockDivider(SPI_CLOCK_DIV16); // slow the SPI bus down
SPI.setBitOrder(MSBFIRST);
SPI.setDataMode(SPI_MODE1);
Serial.begin(115200);
}
void loop() {
// go through the six channels of the digital pot:
for (int channel = 0; channel < 256; channel++) {
// change the resistance on this channel from min to max:
writeSPI(channel ,sinewave[channel]);
// wait a second at the top:
delay(100);
}
}
void writeSPI(byte channel ,byte value) {
// take the SS pin low to select the chip:
digitalWrite(SELPIN, LOW);
// send in the address and value via SPI:
int output = value;
SPI.transfer(channel);
SPI.transfer(output);
Serial.println(output);
// take the SS pin high to de-select the chip:
digitalWrite(SELPIN, HIGH);
}