Other Parts Discussed in Thread: ADS1293
Hi, I'm looking for to use the ADS1293 for an ECG application. ADS1293 has an EMI filter, so only RF noise is filtered. However, there is any protection against defribillation discharge. I wonder which is the best recommendation by TI in order to protect the device. I've looked for 5V TSV supressors, but I saw that, in general, TSV with a max. working voltage of 5V has its max. breakdownd voltage around 7.5V. ADS1293 datasheet has a maximun rating of 6V for the analog operation. I wonder too if it's necessary to include an Oamp buffer separator on each input between the device and the ECG input connector.
I wonder if the schematic attached is well right or it must be modified.
This could be the complete input protection circuit. This include the discharge gas tube and a bidirectional TVS for defibrillator discharge and a separator opamp buffer in order to protect the ADS1293inputs. The example is for one single input lead, so it's necessary to repeat this circuit for all the leads.
I wonder if it is necessary to include or not, or at least a part of this circuit at each one of the inputs of the ADS1293.
please, could you enlight me about this topic ???
best regards, Esteban