Hello,
I want to verify one pin connection I'm making between my PIC and the ADS1298ECGFEPDK. I was about to connect the CLK (SPI) pin of my PIC to the pin labeled SCLK on J3 of the ADS1298ECGFEPDK, but I'm not sure if I should connect it there or to the pin labeled EXT_CLK also on J3. Also, is CLKSEL accessible through J3 as well, or is it represented by JP23 ? I've delegated a pin on my PIC to control CLKSEL, but if it is only accessed through JP23, how I would be able to connect my pin to it?
Thanks,
Noel Teku