This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reg: DAC5688 output harmonics...

Other Parts Discussed in Thread: DAC5688

Hi I am using DAC5688 in my design with following settings...

PLL off

DAC_CLK = 480MSPS

DACDATA_CLK = 120MSPS

Interpolation = 4,Invrse Sync Off,QMC gain/phase Off,QMC offset off,coarse_gain = 0xFF,mixer_gain off

NCO = 45 MHz,Sync = SIF_SYNC

At the analog output I am using the configuration of Fig47 in the data sheet.

I am trying to analyze analog output through DAC_SELF test mode using serial_dac_data register in DAC.I am configuring 0x7FFF as data.

At analog output second harmonic of 45 MHz is just 15 dB down the fundamental.

If I configure 0x5FFF it is 20dB down.

Why there is a presence of such high harmonic of IF frequency??