This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1256 Gain and Offset specs needed for buffer disabled mode

Other Parts Discussed in Thread: ADS1256

I am using the ADS1256 with PGA gains of x1, x2, x4, x8, x16 and with the internal buffer disabled. Can you provide the following specifications for each of the PGA ranges...

1. Offset and Offset drift

2. Gain and Gain drift

Thanks.

  • Hi Tony,

    I would estimate the errors for the other PGA gains as follows...

    • The offset error is on the level of the noise after calibration. Refer to table 4 to get the noise/offset error for the various PGA gains with the buffer disabled.
       
    • The the offset drift will be somewhere between the gain = 1 and gain = 64 cases, because offset drift is an input-referred value that tends to get smaller as the gain increases. For example, the offset drift for gain = 2, is likely to be slightly larger than the offset at gain = 1 divided by 2.
       
    • Gain error is only specified for the buffer enabled; however, as the buffer is another possible source of error, I would only expect the gain error to improve (or remain about the same) by taking the buffer out of the input signal path. The gain error for the other gains will likely be in range of the gain = 1 and gain = 64 cases.

    ...This assumes that the input signal source has a low output impedance! The source's output impedance and ADC's input impedance may create a resistor divider effect that causes an additional gain error when the source's output impedance is high.
     

    • Gain error drift appears to be constant for gain = 1 and gain = 64. I would expect similar performance for all gains.
       

    Best Regards,
    Chris