Other Parts Discussed in Thread: ADS131E08S, ADS131E08
On page 7 of the ADS131E08S specsheet, the internal reference accuracy is listed as +/-0.2%, but the 4V nominal reference min/max limits are 3.88/4.12V, which amounts to +/-3%. Both are spec'd at 25C. Which is correct, or am I missing something?
For comparison, on the ADS131E08 specsheet, the 2.4V min/max limits are 2.394/2.406V, which are much closer at +/-0.25% (accuracy also spec'd at +/-0.2%).