This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7728, fired, help

Other Parts Discussed in Thread: DAC7728, OPA2277

Hello, 

I made a board with a DAC7728, used in bipolar mode (±15V).  Vref is 2,5V, gain is set to 4x.

But some of this chips is fired  in some PCB boards. I found the fired line is  ±15V. So, I am afraid the power supply line is too thin to incur this problem.  

But the line for this chip can not larger than 11 mil, how can I solve this problem or how can I improve the layout in the new design version?

Thanks!

  • Hi Yuanping,

    This seems like a very serious issue.

    I believe that 11 mil should be enough to deliver enough current to the DAC7728 so I don't think this would be the issue.

    To start I will need some basic information:

    • Schematic (List power supplies and voltages at pins, if not clear in the schematic)
    • Layout
    • When does the fault occur? (power-on, when writing to the device, etc)
    • What is the current limit of your power supply?
    • What is the failure percentage right now?
    • Can you send me a picture of a broken board?
    • I would also like to have a picture of the device markings.

    If you would rather discuss this information in private, is it okay to contact you through your E2E registered email?

  • Hi Eugenio Mejia,

    Thanks for your kind response and help!

    The PACKAGE is TQFP-64. The +15V pin is 41 and 8. The -15V pin is 38 and 11. pin 54, 30, 25 are DGND and pin 9, 40 are AGND.

    This accrues when the power-on. At the beginning , small sparks will be found around pins 38 to 41 or pins 8 to 11. If I do not stop the power, smoke and fire will be found.

    The current of power supply is +15V==1A; -15V==0.5A, which gives power to one DSP28335 , eight opa2277 chips and one DAC7728.

    The failure percentage is around 50%.

    My email is ypxu@nuaa.edu.cn and I'd like send the layout and pictures through email.

    Thanks again for you help.
  • This conversation has been taken offline.