Hi,
I have a question about the VPP/VNN maximum rating of LM96551.
In the datasheet of LM96551:
In page 4, it says
while in page 5, it says
So, what is the range of VPP? -0.3V to 55V? 3.3V to 50V? Can I use a voltage such as 1V which is below 3.3V?
Thank you.
Frank