This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can TSC2017 RESET PIN floating or connect to VDD directly.



Hi Bros,

Consider the low distance between two pins, it may improve the PCB cost if we need connect RESET pin to the outside. Could we left RESET PIN floating or connect to VDD directly? Does the internal of the reset pin is an comparator?

Thanks. 

  • Hi Marin,

    If you really want to do that, connect the RESET pin to VDD through a 20k resistor.

    Andy
  • Hi Andy,

    Tks for your reply.


    Sorry not so clear in my question: We are considering connecting RESET pin to VDD directly under our IC' WCSP package to save cost.

    If we connect RESET pin to VDD with a 20K resistor, we need connect the RESET pin to outside which will improve the cost?

    Does RESET pin is one input of comparator inside our IC? I saw some power device is the comparator block.


    Many thanks for your help.