on page 15 of the specification (table 4.3 recommended operating conditions) the maximum Vin +/- voltage range is 2.4V (DC coupled input). The stated Vin +/- differential voltage range is also stated as 2.0V (DC coupled at 20% duty cycle). Lastly, the Vin+/- power is stated as +15.3 dBm (AC coupled mode) and +17.1 dBm (AC coupled mode not maintaining common mode voltage).
Can you please explain why the differences between DC coupled (2.4V = +11.5 dBm) and (1.0V = +10 dBm) (DC coupled at 100% duty)? I'm making the assumption that the voltages in table 4.3 are peak-to-peak voltages in a 50 ohm system. Does the "DC coupled" mode imply 100% duty factor of the input waveform?
Also, can you explain the distinction between the power levels (15.3 and 17.1 dBm) for AC coupled modes (i.e. not maintaining versus maintaining common mode voltage) what does this mean? Thank you.