Hi,
Attached is the ckt which i had made using DAC8760. I want that I can operate it either on dual supply or negative supply depending upon reuirement.
In attached ckt, if dual supply operation is required then I can use it as it is
& if I require single supply operation I will short GND & VSS pin of connector J4.
Is it ok? Or anything else is reuired for above required operation.
Any other comments on ckt attached.