I'm driving an ADS62P49 CLKP/CLKM with a 20.5 MHz signal, believed to be close to 50% duty ratio. On the CLKOUTP/CLKOUTM, I am getting a 20.5MHz signal with a 13% duty ratio. I have set the Low Speed Mode via a register bit.
Couldn't find a spec for this in the datasheet (only listed "typical" duty ratio for a sampling frequency greater than 100 MSPS). Is this low duty ratio normal for a lower sampling rate?