This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC34SH84 Evaluation Module DAC-FMC Adapter does not fit

Other Parts Discussed in Thread: DAC34SH84, FMC-DAC-ADAPTER

Hello,

I recently purchased a DAC34SH84 EVM board and a FMC-DAC-Adapter to connect the EVM to a FMC connector on a Xilinx board. The problem is that the DAC34SH84 has a 180 pin HSMC connector, but the FMC-DAC-Adapter card has a 160 pin HSMC connector. The two do not mate. The description of the evaluation board on the website says " The FMC-DAC-ADAPTER board available from TI enables the connection of the DAC34SH84EVM to the FMC header on Xilinx based EVMs."

I have looked for an alternative TI FMC adaptor card but none are suitable. Is it possible to obtain such an adaptor card?

Thanks for your time,

Andy