Data sheet power for ADS54J69 doesn't seem to match the current/voltage settings...Typical power is 2.66W, but typical V*I = 2.48W. Max power is 3.1W, but max V*I = 3.58. We need to be able to accurately predict our system power, but with the differences between power and input V/I it is difficult to determine how to estimate as well as how accurate the estimate is. Please provide some details why P and V*I are different and why the typical V*I is lower than typical P and why max V*I is higher than max P.
Thanks - Eric