Other Parts Discussed in Thread: THS1207, THS1206
Hello,
I am using a THS1207 in a project and I want to know if I can use an external reference on pin REFIN, or is it mandatory to connect pins REFOUT and REFIN together, and if I want to use an external reference, I must use the differentian reference pins REFP and REFM?
Also, in the datasheet, it is recomanded to use a 10uF capacitor on each REFP and REFM pins. Do I have to use these capacitors even if I only use REFIN pin?
Thank you,
Adrian V.