Hello all,
Made a bit of a mistake. I have a ADUM5401 digital isolator where the output voltage was changed to 5V rather than 3V3 rather late in the design stage. The ADUM feeds an SPI bus to a TI DAC7311. The supply voltage is not so much a problem, but I didn't take into account the signal levels for this (stupid, I know). As a result, if the ADUM output is "on", it rams about 15mA through the ESD diodes on the input of the DAC. To make it even worse, one of the signals is a CS which is almost always high. So, a lot of power wasted and, I assume, an unhappy DAC7311.
The simpelest solution would obviously be to limit the current with a series resistor. I currently have this implemented with a 1k resistor which limits the current to about 1mA or so. From what I can find, this is a safe value for most/all ESD diodes out there. This is, however, a design that is supposed to opperate in harsh conditions for a long time and so my best guess isn't exactly enough for this project. I know some datasheets that list max permissible current through the ESD diodes, but the DAC7311 sheets don't mention it.
Is there a TI bloke out there that can close the loop on this one?