Hi - have a power sensitive application where we are using DAC38J82. The total JESD input rate required for the mode we are using is 9.6 Gbps. For this rate, we could design with 1, 2 or 4 JESD lanes - would you please provide estimates of Ivddt09 and Ivddr18 for each mode to allow us to perform a system level power trade? (the FPGA transmitter is actually lowest power in 2 lane mode)
Thanks - Eric