I would like to use the ADS1158 16-channel multiplexed ADC IC as a high precision (i.e. ideally full 16 bits) for measuring 16 variable resistances using a single-ended supply. Ideally I would like to use a transimpedance amp for measuring the resistance to maintain a constant voltage across the resistance.
The datasheets give a couple examples of circuits on page 42 & 43: http://www.ti.com/lit/ds/symlink/ads1158.pdf
One is for resistance measurement using a bridge, but there are two limitations for my applicatoin: (a) it is a bipolar supply, and (b) it only allows measurement of 8 resistances (since two inputs are used per bridge).
The second circuit is for a unipolar supply, but is for measuring voltages only and seems to use an instrumentation amplified type of configuration between MUXout and ADCin.
Can anyone suggest the best way to modify the second circuit using a transimpedance amp on the MUXout and yet use as much of the ADC's range as possible?
Thanks