Other Parts Discussed in Thread: DAC39J82
Hi,
I am trying to use two DAC39J82 to transmit two identical sinusoidal signal.
By turning off the full complex mixer inside the DAC39J82. I see that the two sinusoidal signal are always in phase between power cycles.
By turning on the full complex mixer inside the DAC39J82. Between power cycles, sometimes I see the two sinusoidal are in phase, sometimes I see the two sinusoidal are 180 degree out of phase. the odds is 50 percent. I am using the sync_out from JESD to sync the nco and mixerab. I have been stuck for a while trying to find out why but fails. by the way, I am using the full complex mixer, and turned off the QMC module.
Do you have any suggestions?
Thanks a lot.
Hao