Hi,
I am using ADS1110 16-bit A/D converter to convert differential and single inputs coming from different sources.
In differential input mode where the signals are generated across the thermal disk (thermal power converted to analog voltage), I don't see the digital data. Even analog input across the ADC i/p pins are changing (0.65mV/1.30mV/2.60mV). Here I could see the source which generates analog signal is passive source (Peltier module - it converts temp difference to voltage difference across its terminal).
However ADC is working perfectly when analog input is generated across a shunt resistor connected in series with photo diode.
In first case where source pwr/gnd is not connected to the pwr/gnd of the ADC, I notice the issue of not converting the analog values - is this happening due to common mode voltage spec is violated. Do we need signal conditioning prior to the ADC? Current circuit implementations look like below:
Please let me know why ADS1110 unable to convert the analog inputs, what is wrong with the circuitry?
Awaiting your valuabe inputs...
Thanks & Regards,
Rajesh