I am currently building a 1 off based on the ADS1278, following the ADS1278EVM. I would simply use the evaluation board however my application needs at least 6 channels buffered, and also needs the buffer gain adjusted to deal with a +-10V bipolar input.
I have already viewed the following:
https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/108440
http://www.ti.com/lit/an/slyt336/slyt336.pdf
https://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/190521
http://www.ti.com/lit/ds/sbos458h/sbos458h.pdf
I have the following requests/questions:
1) Are gerbers available for the THS4521EVM, described in this datasheet: http://www.ti.com/lit/ug/sbou080/sbou080.pdf
2) The layout for the THS4521 amps as used in the ADS1278EVM seems much relaxed as compared to that on the THS4521EVM. Is this because of the low frequency use?
3) The buffer circuit used on the ADS1278 is also shown on the front page of the THS4521 datasheet. A simple DC analysis shows that a the buffer circuit will take a +-2.5V single ended input (Vin- held at 0, Vin+ is bipolar) and convert this to a proper differential output centered on the Vocm value; without exceeding the common mode limits of the amplifier. Is my analysis correct?
4) For low frequency use (below 100kHz) can I simply change the input (Rg) resistors from 1K to 4K to deal with my +-10V input range?
5) Can the 1.5nF capacitors be safely increased to roll off gain at a lower frequency? My highest frequency of interest is 25kHz, and I was thinking of using 15nF rather than 1.5nF.
Many thanks
Jonathan Edelson