Other Parts Discussed in Thread: AFE4403
Dear all,
I've recently bought an AFE4403 Watch EVM to develop custom PPG processing algorithms. It all appears to work well with the provided GUI, but when I try to record data "on the field" without an USB connection, then I don't know how to download the content of the flash to the PC.
I looked into the firmware source code, and I see that data is being logged to the flash, but found no way to read it back. I must surely be missing something very obvious...
I've also found in this forum some documentation on the protocol used to communicate over the USB-emulated serial port, but found only register-setting commands, calibration commands, and the like used by the GUI, nothing to read back the flash.
Any help will be greatly appreciated. I can write a custom program on the PC to implement the protocol if any documentation is available.
With best regards,
giorby.