Other Parts Discussed in Thread: ADS1232REF, TUSB3410
I have an ADS1232ref instrument that is reading measurements from a load cell (Honeywell 31 load cell, 500 gram range, vacuum operation). I am reading the values in labview. After some time in operation, the board shuts down unexpectedly. After it shuts down I have to turn it back on with the reset button. When fast mode is turned on, the board shuts down quicker compared to when it is running in slow mode.
I checked my port settings and I have the option to "turn off the USB when it is consuming too much power" off. I also added a wait time before the write and reading operations.
My gain is set to 1 with an input voltage of 5V.
I am not sure what is causing this problem so any advice would be greatly appreciated.