Other Parts Discussed in Thread: AFE5809
Hi,
I'm having trouble configuring the AFE5809 decimation filter.
I'm using the following coefficients take from a previous post for say decimation by 8 filter
uint8 pu8_fircoeff_DEC8[8 * 14]={
0x0F,0xEF,0xFC,0x60,0x06,0xBF,0xF1,0x00,0x23,0xFF,0xC0,0x00,0xBF,0xFF,
0x0F,0x1B,0xF6,0xF0,0x11,0xBF,0xD9,0x00,0x5B,0xFF,0x50,0x01,0x7F,0xFD,
0x0D,0x8B,0xF3,0xE0,0x18,0x3F,0xCA,0x00,0x7B,0xFF,0x00,0x01,0xFF,0xFD,
0x0B,0x5F,0xF3,0x10,0x1A,0x7F,0xC5,0x00,0x87,0xFE,0xF0,0x02,0x3F,0xFC,
0x08,0xCF,0xF4,0x50,0x18,0xBF,0xC9,0x00,0x7B,0xFF,0x10,0x01,0xFF,0xFC,
0x06,0x13,0xF6,0xF0,0x13,0x7F,0xD4,0x00,0x63,0xFF,0x40,0x01,0x7F,0xFD,
0x03,0x6B,0xFA,0x70,0x0C,0x3F,0xE5,0x00,0x3F,0xFF,0x90,0x00,0xFF,0xFE,
0x01,0x0B,0xFE,0x30,0x04,0x3F,0xF7,0x00,0x17,0xFF,0xE0,0x00,0x7F,0xFF} ;
SLOS738E section 8.6.2.1.3 advises to first write to 0xC6[7:0] with base address, which I have assumed is 0x0000.
It then advises to write 112bits to SPI address 0xC7, MSB first, although its not clear how these bytes are to be written.
i.e. does one convert each 14 byte row to MSB bitstream and send as 112 bits with single address
MSB First LSB Last
e.g. row one is sent as 11000111 00001111 ...... 10000011 1111111
0xC7 0x0F 0xBF 0xFF
or does one have to pack the 112 bit bitstream into 7x16bit transfers each with separate address as per the SPI protocol description in Figure 83 of SLOS738E?
I have tried both approaches but I cannot seem to get anything sensible out of the decimator filter when testing either in coeff test mode or injecting sinewaves using the sine test mode. I can see the sinewave and mixer outputs if I bypass the filter, but one enabled ... nothing..
If I use the ADDRESS + 112bit SPI transfer, I note that 0xC6 increments after each transfer, which I assumed is the expected behaviour. However when I try to test either with test mode sine, or test mode coeff (impulse), the with the decimation filter enabled, the output is zero, regardless of test mode.
I can confirm that in all test cases I perform a '1' write to Register 0 bit 2 (SPI_DIG_EN=0) after performing the RAM writes to load RAM.
I'm at a loss as to what to try next.
Is it possible to readback RAM coeff data to verify it has been written properly ? How precisely would this be done ?
Thanks