This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Bit of a newb with electronics, so if this question has an obvious answer, please excuse me.
I am trying to attach an electronic drum pad to the Vin input of an ADC0820 flash ADC. I am powering it with 5v and using a 3.3v reference voltage (the voltage ref is a differential input on this IC, with a VRef- of 0V. When I attach a 10k pot to the ADC Vin input, everything works as expected.
Here's the thing that's confusing me: when I hook up a scope and read the drum pad when it's not attached to the ADC, it reads at 0 Volts when not being hit. However, when I attach it to the Vin input this level rises to 0.1 Volts and causes the ADC to read above 0. It seems the Vin pin is charged from the VRef+ pin and this is being sent back down the drum pad. I have confirmed this by connecting a pot to the VRef+ pin and turning it up and down - the charge leaving the Vin pin changes! This doesn't happen when I experiment with different ADC chips. Why is it happening here?
Thanks for the help
Dan
This is a Precision ADC - I will move this thread to the correct group.
Ken.