Hi !!!
I am a student and am trying to understand the effects of sampling and aliasing.
I am confused over the the fact that the minimum required sampling rate for band pass signals.
Lets take an example of a signal with:
upper cut-off freq = 108MHz
lower cut-off freq. = 88MHz
Following the example (and formula for finding the allowed sampling rates without aliasing) given at link (https://en.wikipedia.org/wiki/Undersampling)
The minimum allowed frequency is 43.2MHz.
Now, my doubt is the following:
(1) since the example is that of a bandpass signal, any frequency within the upper and lower cut-off is allowed
(2) if i choose a single tone sine wave exactly at upper cut-off freq.(108MHz) , what should be the minimum sampling rate ?? Nyquist rate suggests it should be atleast 2*108MHz or 216MHz.
(3) but as explained in the link the minimum sampling rate can be 43.2MHz.
(4) how can a sampling rate of 43.2MHz be sufficient for a sine wave of 108MHz??
please help me clear this doubt??