Hi,
My cutstomer has question below.
Could you give me answer, please?
Q1: There are "Register 85" and "Register 115"
Which setting is priority high?
Customer uses JESD204B subclass1.
Which mode does ADS52J90 become when "Register 115"(ENABLE_JESD_VER_CONTROL=0) is set to 0 and "Register 85" is set to JESD204A?
Q2: Is there the way to distinguish of "JESD204A or B" and "subclass0 or 1" expect seeing internal register?
Q3: At JESD204B subclass1, Can ADS52J90 send data by only using SYNC, not using SYSREF?
Best regards,
Shimizu