I have an older ADS1278EVM PDK. I can't get past the load to the MMB0. I've searched through this e2e and suspect I need the right documentation so that I can get the switches and jumpers right. The 'vintage' info is
6492528 PCA "E", 6492526 PWB "D", 6492525 BOM "D"
MMB0: Rev "D", 6462011 BOM REV __, 6462012 PWB D,
After loading the EVM package the ADCPro fails, instructs to reset the HW (which has no apparent effect) and eventually times out ; failing to load the MMB0.
Then the following message appears:
An error occurred with error code 6070 libmmb0.lvlib:EEPROM READ .VI <err> unable to Read from EEPROM.
Looking closely at the MMB0 I think I can see solder bridging on some of the DSP pins. I'll try fixing the bridges if I don't here advice against that.
The instructions indicate that damage can occur if the unit is powered with the wrong jumpers and switch settings. What, specifically, might be damaged? I wouldn't want to invest too much time before popping for a new one.
Thanks for reading