This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Clarification request regarding ADS1298, 4KSPS datasheet

Other Parts Discussed in Thread: ADS1298

Hi

I have 2 queries:

Query 1:

Please let me know if the 4KSPS Data rate mentioned in graphs of the ADS1298 datasheet, is for SINGLE Input channel of ads1298 or ALL 8 input Channels.

My confusion arises because above the figures (as in Figure 9. PSRR vs Frequency) the datasheet says:

at T A = 25°C, AVDD = 3 V, AVSS = 0 V, DVDD = 1.8 V, internal VREFP = 2.4 V, VREFN = AVSS, external clock = 2.048
MHz, data rate = 500 SPS, high-resolution mode, and gain = 6 (unless otherwise noted)


If I consider 500 SPS for single channel.. then 500 x 8 channels = 4ksps.

Query 2:

Under Section 1. Features:

Data Rate: 250 SPS to 32 kSPS

is mentioned. Please let me know if 32 Ksps is Possible on SIngle Input channel . 

Or is it a product of 4Ksps (per input channel) x 8 channels = 32ksps.