Hi,
I haven't installed vcxo to the evm. I applied a 200mhz clk from my artix 7 kit io pins . As given the vcxo_in signal should be 1vpp with 0 volts dc, so i applied a voltage divider. but the evm is detecting the clock only at 3.3v peak to peak not less than it.
What could be the reason and is it safe to apply 3.3vpp to vcxo_in?