Other Parts Discussed in Thread: DAC3484, DAC34SH84
Dears.
We are testing with DAC3484
We would like to inquiry about DAC3484 of PLL.
VCO RANGE is 3.3GHz ~ 4.0GHz by Datasheet.
But as we input 4000MHz in below formula, Coarse tuning bits is out of setting range.
So we have no choice, only set Coarse tuning bits to 63 can read pll_lfvolt(2:0) to‘0’.
Please help to check how can use PLL with 4000MHz VCO Frequency.
** Please refer to the below PLL parameter.
DACCLK is 200MHz.
Target-Frequency is 800MHz.
Interpolation is x4.
|
fVCO |
4000 MHz |
|
PFD |
40 MHz |
|
N |
5 |
|
M |
20 |
|
P |
5 |
|
pll_vco |
63 |
|
P*M(=overall divide ratio) |
100 (single charge pump) |