Hello:
I just got ADS1293 EVM board. I am confused about the settings of the board. I have the following confused status?
1. Do I need to connect a battery at JP1 while I am connecting the board with PC using USB . If yes, what volt I have to add, is it 3.3v or 3.6 V? What is the VDD_INP and VDDIO connector for?
2. Why 8 GND connector there, Do i have to connect ?
3. what kind lead I should use, Can I use simple wire.
I appreciate your quick answer. Thank you