Other Parts Discussed in Thread: ADS1262
We try to design a 4-channel system with ADS1262 to do sampling at exact same time (not multiplex). We connect single clock 7.3728MHz, and single START signal to four ADS1262s. The chip works under continuous mode, Fs 38400Hz. We observe that the time of the first falling edge of DRDYs between difference ADCs after enabling START varies between 4~5 7.3728MHz cycles. The datasheet gives the latency is 0.207 sec which is only in the precision of millisecond. Can TI provide more precise latency performance, like in microsecond?